Part Number: LDC1614 Other Parts Discussed in Thread: TMUX1136 We are working on an application that identifies inductances in the order of ~200nH, With series resistances of ~0.5Ohm.
Due to the relatively low quality factor we need to use the LDC1614…
Part Number: LDC1614 Hello team,
Can you answer the questions from my customer?
1. What is the signal processing at the core of the IC?
2. In the past, I heard that the round shape of the sensor works better at higher frequencies than the square shape…
Part Number: LDC1614 Hi expert,
my customer is using LDC1614 and they want more guide about:
1. how to minimum the influence of temp when using;
2. how to minimum the influence of mechanical jitter when using;
3. tips of improving the EMC;
Part Number: LDC1614 Hi Team,
The change in displacement is measured using the LDC1614. Using the PCB coil as the sensor, the LDC1614 count changes abruptly away from the metal object, as shown in the following figure:
The PCB coil is moved by fixing…
Part Number: LDC1614 Other Parts Discussed in Thread: TCA9416 Hi
I have a PCB which uses a NFC tag as a I2C bridge for communication and power supply to the LDC1614RGHR sensor. I have only one master (tag) and one slave (sensor) at the I2C lanes. If I…
Part Number: LDC1614 I'm a student in Taiwan and I bought your LDC1614. However, I have a problem about the sensing points which are output to Excel. In the normal condition, the sensing points according to the sample rate setting on EVM GUI can calculate…
Part Number: LDC1614 Hi TI team,
I am working on a design to sense small metal objects such as drill bits using an LDC 1614 board. The board is using 2 ICs with 4 coils on each IC. The goal is to have one or more coil to sense one object ideally and have…
Part Number: LDC1614 Hi Team,
We use two LDC1614 for detecting 8 steel rode of 6mm each.
The antennas we're using have 22 turns and 4 layers, with an external diameter of 16mm and an internal diameter of 2mm. Our bulk capacitor is a 470pF in X7R. The…