Part Number: LINUXSDK-OMAPL137
Tool/software: Linux
Dear Sir/Madam,
I am working on OMAPL137EVM board. I want to use SPI1. I configured linux to build SPIDEV. It seems that I should also change pinmuxs 8 and 9. I do not have access to these registers…
Part Number: LINUXSDK-OMAPL137 Other Parts Discussed in Thread: OMAP-L137
I understand this is a bit strange but I've been trying to re-build uboot u-boot-1.3.3 from REL_LSP_02_20_00_07. I have been able to fix all compilation errors due to gcc 7 not…
Part Number: LINUXSDK-OMAPL137 Tool/software: Linux Hello Community,
I have a arm application which inits syslink and start the dsp application. They communicate over MessageQs between each other which works fine.
Then I have a second arm application…
Through syslink you can communicate to DSP from ARM.
So you have to use the older kernel version (2.6.37) not MCSDK.
Yes, montavista toolchain can be used for your development.
www.ti.com/.../linuxsdk-omapl137
Vincent,
The OMAPL137 EVM have the audio codec (AIC3106) chip. It supports the speaker equalization. Refer the datasheet of AIC3106 . In addition that, please have look at the technical reference guide to get more details of OMAPL137 EVM. http://www.ti.com…
Hi Samuel,
Welcome to the TI E2E forum. I hope you will find many good answers here and in the TI.com documents and in the TI Wiki Pages . Be sure to search those for helpful information and to browse for the questions others may have asked on similar topics…