Part Number: LM124AQML-SP Hello,
For the LM124AWGRQMLV I was wondering if applying ~2.5V to the non-inverting input while the device is unpowered is a safe condition or if this might cause damage. Thanks for your help!
Best,
Adam
Part Number: LM124AQML I am reviewing the "MIL_QML" product and I don't know how to check the "Qualification Status". let me know . And I also want to check "Quality Level". How can I do it?
Part Number: LM124AQML-SP Other Parts Discussed in Thread: LM324 , LM358 Hello,
I was wondering ifapplying ~2.5V to the non-inverting input of the LM124AWGRQMLV while the device is unpowered is a safe condition or if this might cause damage. Thanks for…
Part Number: LM124AQML Hello,
concerning the LM124AWRLQMLV, it is available per SMD with 2 variants:
- High Dose Rate: 5962R9950401VDA
- Low Dose Rate: 5962R9950402VDA
I read in the SMD that:
"The manufacturer supplying RHA parts on this drawing has completed…
Hey Yves,
Was the issue resolved? I will mark Kai's answer as "TI Thinks Resolved," please confirm. If the issue isn't resolved, please let us know so we may further assist.
All the best, Carolina
Part Number: LM124AQML Other Parts Discussed in Thread: LM124 Hi,
In the datasheet of the LM124AQML the output voltage swing is given at (V+)-1.5V in the features and further in the document is given at Voh 26V or 27V according to the load for V+=30V…
Layout 1 is an old datasheet from National Semiconductor, but it is the current version linked from the LM124AQML product page ("Die D/S").
Layout 2 is the current version of the LM124-SP datasheet, but note that "LM124 MD8" is an orderable…
Part Number: LM124AQML Other Parts Discussed in Thread: LM124 For the 5962R SMD LM124 devices what die passivation is used? Also, is the passivation layer the same for the ELDRs and non-ELDRs but rad-hard LM124 quad op-amps?
Thank you,
Alan Kurdziel