Part Number: LM15851EVM I'm testing an LM15851EVM attached to a TSW1457J capture board. It runs successfully with decimation of 8 and 16, but not with a decimation of 10. On the LM15851EVM Decimate-by-10, DDR is selected. In HSDC Pro LM15851_D10_DDR is…
Part Number: LM15851EVM When trying to connect to the evaluation board the LM15851 GUI v1.2 has an error "FTDI Device not connected properly". FT_DEVICE_NOT_FOUND I've reinstalled the USB and attempted to update the FTDI device using FT_Prog (using file…
Part Number: LM15851EVM Tool/software: Linux Dear TI support,
I have ZCU102 Kit and LM15851EVM kit. I would like to connect directly LM15851EVM to ZCU102 but I am not sure they are compatible or not.
Please help to confirm with me
1. ZCU102 and LM15851…
Part Number: LM15851EVM Hi!
Can you tell me please, why did you place the LM15851 on the opposite side of the board?
Thanks in advance!
Best regards, Vic.
Part Number: LM15851EVM Hi!
The LM15851 datasheet states that each NCO_x pair must be connected together and driven with a common 1.8V LVCMOS signal (but, as it's seen in the Pin Functions table, these inputs appear to have differential structure). In…
Part Number: LM15851EVM Hi!
I'm designing a power supply network for an RF-sampling wideband receiver and use the LM15851EVM as a starting point. As such a system requires well filtered low noise power supplies for the sensitive devices used, the ferrite…
Other Parts Discussed in Thread: DAC38J82EVM , XEVMK2LX , RFSDK My customer is trying to connect both LM15851EVM and DAC38J82EVM to XEVMK2LX simultaneously. They use LFMSHD = 22210 mode. They created their own driver (USE-CASE-CUSTOM) based on the existed…
Other Parts Discussed in Thread: LM15851 , ADC12J4000 Hi team,
we’re working with a ctm testing LM15851 to develop an high speed data converting system.
They’re evaluating it through TSW14J10EVM and LM15851EVM.
We know there are a few version…
Other Parts Discussed in Thread: LM15851 I'm working through the slau561a guide to getting this evm working. The lm15851 gui appears to program the clocks and ADC correctly, the foreground CAL also seems to finish without complaint. In HSDC the lm15851…
Hi Vic
The basic concept of what you need to accomplish is shown in the figure below. The LMK048xx device is needed to create the FPGA clocks and SYSREF for FPGA. It can also create the ADC SYSREF if that signal is needed. The LM15851 can operate without…