Many thanks for the review
R201 is not populated (done by BOM)
current limit is set bei 18k (Iadj) should give 2A limit according the data sheet, or is my assumption not correct?
V201 is a MBRS3200, schottky with 3A rating
L203 rating is 4.5A, saturation…
Part Number: LM22673-Q1 Hi Team,
I am looking into the mean time between failures for the LM22673-Q1, and I noticed an odd curiosity of the part.
According to the table below for the device, it states that the estimates are made off of 1703 data samples…
Part Number: LM22673 Other Parts Discussed in Thread: LMQ66430 , TPSM63603 Hi team,
We've got the question about the thermal registance of LM22673. Do we have ψJT of LM22673TJE-5.0/NOPB(TO-263) ?
Regards,
Toshiaki Morita
Part Number: LM22673 Hi Team,
If soft-start function is not needed, what to do with this pin? What will happen when floating this pin? Thanks.
BRs,
Francis
Part Number: LM22673 Dear Sir/Madam
We have purchased a TI part LM22673MRX-ADJ/NOPB,DC is 2141+ COO MY,but we do X-RAY,found that the leads frame and wire bond not same as before 19+ one,COO was PH.
And the marking format are different also.I can't find…
Part Number: LM22673 Does the LM22673MRX-ADJ/NOPB have an enable pin? The functional block diagram on page 8 of the datasheet shows that it does, but the pin description doesn't show one. Also is this part recommended for new designs?
Part Number: LM22673 Hi Experts,
Good day.
Due to supply shortage, our client would like to use LM22673MR-ADJ/NOPB as an alternate to the LM22670MR-ADJ/NOPB, but we're not sure if it would work as they have different pin fxn at pins 3&5.
A more…
Part Number: LM22673 Hi, support team
My customer has the questions as follow:
What is the maximum value of output voltage overshoot when the input voltage chattering?
For example, when the input voltage between 4V and 5V changes to 20V ~ 40V, the output…