Part Number: LM25037EVAL Other Parts Discussed in Thread: LM25037 Hi guys,
I'm thinking about using the LM25037QMT to design a boost converter that would take a 12V input from my battery and convert it to a 24V output.
I want to use a topology of an…
Part Number: LM25037EVAL Other Parts Discussed in Thread: LM25037 Hi TI Team I have got your LM25037EVAL board. after verify function i have some question about softstart circuit. In schematic use SS Cap = 0.68uF. So T3 should be around 27mS. but…
Part Number: LM25037EVAL Other Parts Discussed in Thread: LM25037-Q1 , , LM5022 Hello,
I'd like to use the LM25037-Q1 in a vehicle CDI power supply design:
6V < Vinput < 32V
===============================================
Vout = 280V
0.1A < Iout…
Part Number: LM25037EVAL Other Parts Discussed in Thread: LM25037 Customer ordered the EVM,but didn't mange to operate it above 1.5MH (750K each ).
What could be the reason?
Hi Kuramochi-san,
Unfortunatley there is no evm for the LM5037, the device is similar to the LM25037 which has an evm based on push-pull topology. You can directly replace the controller to evaluate the LM5037 on the LM25037EVAL. If you want to evalutate…
Other Parts Discussed in Thread: PMP , LM25037 , LM25037EVAL Hello,
i found the DEV Kit PMP7797 which is the right part for a project on which i'm working.
Where can i buy this part ?
Best Regards,
Martin