Part Number: LM25069 Other Parts Discussed in Thread: TPS25990 , , LM5066 Tool/software: Hi
The current design requires 110A for 12V output If you want to meet 12V 110A as shown in the figure Is it possible to solve the problem by increasing the number…
Part Number: LM25069 Other Parts Discussed in Thread: CSD16415Q5 , Hi team,
We are validating a reference circuit for LM25069PMM-2 that was given to us by a customer.
Under the following conditions.
Could you please tell me if there is a problem…
Part Number: LM25069 Hi Ti Friends,
I use LM25069 as the hot swap controller equipped a manual reboot circuit.
When I press the button SWT1 to lower the voltage of the PIN_UVLO/EN, LM25069 will off the MOSFET.
Where VDD3V3 is converted by a D-D…
Part Number: LM25069 Other Parts Discussed in Thread: TPS2595 , TPS2597 Hi Team,
Our customer is using the LM25069 in their board and would like to ask for a review. Kindly refer to the details below:
For Vsys=12V, I will put that hot-swap controller…
Part Number: LM25069 Hi Team,
Our customer is considering LM25069 as a load switch for a power supply that have very large capacitors.
Vin to LM25069 is 13V
Vout from pass transistor can be down to 12.7V
I load max is 5A max
Cload is 5200uF…
Part Number: LM25069 Hi, LM25069_Calculations_17May2022.xlsx
Our design uses LM25069PMM-1.
During the tests we have found that the Inrush control circuit stopped working after few power ON / OFF & Load Turn ON/OFF cycles.
GATE voltage is stuck to…
Part Number: LM25069 Other Parts Discussed in Thread: TPS2597 Hello Team
Is LM25069 suitable for use as a general purpose e-Fuse ?
I want to use it for input protection of my circuit board which has mixed signal IC's and resistive and inductive loads…
Part Number: LM25069 Hi,
Our design uses LM25069 hot-swap controller.
Following are the design inputs for which the hot-swap controller to be designed:
Vin (min/typ/max): 11.5V/12.1V/12.5V
I(max): 44A
Rsense: 0.75mOhms (two 1.5mOhms in parallel…