Part Number: LM25069 Other Parts Discussed in Thread: TPS25982 Hi team
TI P/N: LM25069PMMX-2
Input voltage: 5V or 12V
Load current: 5A, 10A, 15A
My customer wants to know whether they could use 0402 package resistors and capacitors for the external…
Part Number: LM25069 Other Parts Discussed in Thread: TPS25982 , CSD17570Q5B , CSD16415Q5 Hi team
Could you help check if LM25069 + CSD17570 is suitable for 16.5A Iout application?
Vin=12V&5V
Iout=16.5A
The customer prefers to hot-swap device…
Part Number: LM25069 Other Parts Discussed in Thread: LM25066 Hi Guys
Our customer is using our LM25069-2 as Hotswap application. 12Vin, 12Vout. They tested the current limit operation:
1. Normal room temperature: CH2: 12Vout. Ignore CH1; We can see…
Other Parts Discussed in Thread: LM25069 art Number: LM25069
Dears,
I use LM25069 in my product, as below mode, The Under-Voltage Lock-Out is 4.5--4.53V, and Over-Voltage Lock-Out is 5.5--5.53V.
As my DCDC power module for Vsys = 5V needs 5mA…
Part Number: LM25069 Hello Expert, I have question regarding LM25069. I'd like add external current sens amp for IRIM resister between VIN and SENSE. I think there is any problem if input impedance is sufficiently high but I'd like to confirm whether…
Part Number: LM25069 Other Parts Discussed in Thread: LM5069
Hi, Is there an upper limit value for the capacitor connected to the gate pin? Our customer connects 1μF capacitor. Also, 1 kΩ is connected in series with the gate of the MOSFET. is there…
Part Number: LM25069 See my question in the title.
I use LM25069 on a power supplier board, while my upstream DC/DC converter has build-in over-current protection functionality, in such senario, Can I just delete the current sampling resistor(R30 in…
Part Number: LM25069 Hi, I will ask you questions related to the previous question. Due to the large capacitance of the gate pin, can it be stressful for the inside of the LM25069? When the capacitance value of the gate pin is 1 μF, between GATE and GND…
Hi Praveen:
Thank you for your quik response.
Yes, I just need a ideal doide, one of your FAE recommand the LM5050 to me, but I want to know if it's apporiate to use LM25069, as the duaghter card use the LM25069 as hot swap controller, so I can get…