Part Number: LM2595 Hello all.
I am facing some problems with this IC.
My input is around 28 V and my circuit is:
In some tests, it seems that the LM cannot start and the operating frequency drops to 8kHz and the voltage does not reach 5V (it stays at…
Part Number: LM2595 Hello,
Can you please explain me what are the main differences between de following Power Conventors:
LM2595SX- ADJ /NOPB and LM2595SX- 5.0 /NOPB
Regards,
Kathleen
Part Number: LM2595 Hi!
My customer is using this device and wants to clarify requirements for the output capacitors.
"Do not use capacitors larger then 330uF". Does this mean a single capacitor cannot exceed 330uF? Or that the whole 5V output rail cannot…
Part Number: LM2595 Hi,
The datasheet from the LM2595 ( revised may 2016 ) shows at paragraph 8.2 the Functional Block Diagram.
Within this diagram the feedback resistors R1 and R2 have different values dependending on the version. E.g. for the 3…
Part Number: LM2595 Hi,
This question regarding the IC LM2595S-ADJ/NOPB.
We are using this regulator in our existing design. At present we are doing a safety testing for our instrument [where this IC is used]
This IC comes under the limited energy circuits…
Part Number: LM2595 Hi Team,
Rated power dissipation not mentioned in datasheet
Please share us the rated power dissipation so as to check derating.
Awaiting response
Part Number: LM2596 Other Parts Discussed in Thread: LM2595 Datasheet for LM2596 rev C SNVS124C has correct absolute maximum table for the part.
Since rev D and onwards, the table is for the wrong part.
Current rev G continues to serve the wrong information…
Part Number: LM2595 Hi team.
I'd like to change input voltage 24V to 12V as output voltage is 12V.
*Because the input voltage changes with time.
Is it possible?
I can not simulation on webench.
Sincerely.
Kengo.