Hi Harry and Niklas,
Thanks for your suggestions. As of now, I would like to work on LM2611 testing. I will update you on the test results on the another thread.
Part Number: LM2611 Other Parts Discussed in Thread: TIDA-01457
I need a -3.81 .1A typical, .15A max regulator. It will power RF circuitry, so it needs to be quiet as possible.
I’m more of a digital designer, and definitely out of my comfort zone with…
Part Number: LM2611 Hi,
We want to provide some delay in the output voltage start up for +5V to -5V conversion using LM2611 converter. For providing the delay, we are using a RC network. We have connected 1M and 33nF RC network to the Shutdown pin (SHDN…
Part Number: LM2611 Hello Team,
I can see the Grade A and B have difference in Current limit value.
Is there any reason LM2611 has 2 kinds of current limit? Thank you!
Hi Niklas,
While debugging, I have found the below observation:
Case 1: With the SHDN pin connected to the VCC directly, If I supply 12V at the input to the regulator, the output voltage of the regulator is -4.88V. When I connect a load at the -5V rail…
Part Number: LM2611
Hi team, Kindly review the schematic above motioned , I have used the inductor part CR32NP-150KC Kindly share your feedback..
Thanks Arun
Part Number: LM2611 HI, team:
Could you help select a DC/DC device could support 7vin, withstand voltage 18V,output -5.5V 0.15A .
Hope small size not bigger than SOT23.
Thanks.
Part Number: LM2611 Hi Team,
I have a quick question regarding the LM2611. After reading the datasheet, I couldn’t find a formula for calculating the resistor value to create an output voltage of 8.8 Volts. Would you be able to provide this equation for…