Part Number: LM2623 Hello I have one question.
VDD must input 3-5V. So, if the output voltage is 10V, is it possible to connect the resistor-divided voltage at the output voltage to VDD?
Hi Tommy,
To further check the UVLO issue, could you provide more information? Such as the two question shown below.
Two question: what's the output current? Does " it doesn't work " mean the Vout can't be regulated to 5V or the device can…
Part Number: LM2623 I am finding a replacement material for AP3015KTR-G1(Diodes), witch price is 1.9USD, so aggresive.
Cusotmer need input voltage is less than 1.5V and the output voltage is greater than 12V.
Do we have any recommendations?
thanks.
Part Number: LM2623 Other Parts Discussed in Thread: TPS61376 Does TI have a boost chip similar to the LM2623?
Input voltage 0.9-16V, but But it's cheaper than the LM2623.
Part Number: LM2623 Is there any method to limit LM2623 current? I have 3.6V thionyl chloride lithium battery with max peak current 3A. My 12V circuit draws two 20-40ms high current pulses. Device to device the peak current from the battery varies 2.6…
Part Number: LM2623 Other Parts Discussed in Thread: TPS61022 Hi,
In the datasheet mentioned that the maximum voltage for VDD is 5V and the absolute maximum rating is 10V.
i would like to ask how much is it problematic to push the VDD voltage of 5.5V…