Part Number: LM2623EV Other Parts Discussed in Thread: LM2623 , Hi,
I am designing a battery powered board. My battery voltage drops to 1.6 V. So I wanted to use LM2623 Step-Up Converter (PCB draws 200mA@1.6V). I read LM2623' datasheet and LM2623EV…
Part Number: LM2623EV Other Parts Discussed in Thread: LM2623 , TPS61021A Hi ,
I wish to use LM2623Q1 for a DC/DC converter .
Input : Single cell AAA Alkaline ( 1.5V)
Output : 5V ( max load is ~ 0.3A)
1. is it a good choice ?
Can I use LM2623EV…
Part Number: LM2623EV I have looked at two of the lm2623ev/nopb demo board. I hooked power to first board's inputs and turned on the supply. The power supply folded. My first thought was did blow it up? I ohmed the red lead (vin) to the black lead (gnd…
Part Number: LM2623EV Other Parts Discussed in Thread: LM2623 , Team,
Per LM2623 datasheet startup voltage is 1.1V.
Is LM2623EV board configured in a way to provide an output at that voltage?
My customer cannot get any output below 2.0V. Any input…
Other Parts Discussed in Thread: LM2623EV , LM2623 I just bought a LM2623EV evaluation module. The input was connected to a DC PSU at 3 V. I measured the output using a DMM and expected to see 5 V.
When I turned on the PSU, it showed that the module…
Other Parts Discussed in Thread: LM2623EV I ordered the LM2623EV board. The only documentation there is on this board is this app note:
http://www.ti.com/lit/ug/snva063g/snva063g.pdf
There is a schematic on the app note that doesn’t include several…