Part Number: LM2731 Hi all,
could you please confirm that the LM2731YMF is currently indicated as LTB whereas the LM2731YMF/NOPB and LM2731YMFX/NOPB are Active and will continue to be as such?
Thanks,
Adrian
Part Number: LM2731 Hi Team,
I have a couple questions regarding the LM2731.
The datasheet specifies that a compensation capacitor is to be used to form a zero at 6 kHz in the feedback path of the boost converter circuit.
In my design, the resistor in…
Part Number: LM2731 Hello everyone,
I was wondering if the LM2731XMF/NOPB can output a voltage higher than the 20V max if I reference ground to a higher voltage. Let's say I have 50V at Vin and a ground reference of 40V, would the device the the input…
Part Number: LM2731 Tool/software: WEBENCH® Design Tools Same design was run on webench on 2 different dates this year (May and August). August report now produces much worse results. Pd of controller jumps from 18mW to 50mW for exact same design! efficiency…
Part Number: LM2731 Tool/software: WEBENCH® Design Tools Hi Team,
When simulating the LM2731 in WEBENCH, the working condition is: Vin= 4-8V, Vout=11V, Iout=30mA, the simulation result shows the efficiency is 91.9%.
However, if using LM27313, the simulation…
Part Number: LM2731 Other Parts Discussed in Thread: TPS61040 , TPS61085 , TPS61087 , TPS61023 , TPS61170 Hi Team, I am posting this on behalf of our customer regarding their situation with the different results in the circuit products by Webench design. Here…
Part Number: LM2731 Hi,
I've designed a printed circuit board with the typical application circuit of LM2731.
It is intended to use Vin=5V and Vout=9V. The values of the external components used are:
C1=2.2uF; L1=10uH; D=MBR020L; R1=106k; R2=16k;…
Part Number: LM2731 Hello team,
I use LM2731 in my design.
I want to slow start to reduce inrush current on the power supply when power on,
I add RC on the SHDN pin.
the R=47k, C=1UF,the input power is 5V, output is 12V,I want to delay ~20ms to start…
Part Number: LM2731 Tool/software: WEBENCH® Design Tools Hi team,
Do we have an available model for the LM2731Y (0.6MHz) version? We have a version for the X device, but we would like to model the Y version for transient stability.
Thanks,
Arthur H.
Part Number: LM2731 I see SC4503 can do soft-start by connected SHDN pin on external Rss/Css.
Can LM2731 do the same thing?
https://www.semtech.com/uploads/documents/sc4503.pdf