Part Number: LM27762 Tool/software: Hello,
I'm using the LM27762 to provide +/- 2.75V for precision analog circuitry. I'm trying to decide if the downstream analog ICs' decoupling caps should be differential (between +/-2.75V) or common-mode (each rail…
Part Number: ADS124S08 Other Parts Discussed in Thread: TPSM82912 , LM27762 , Tool/software: Hello,
I am currently looking into power supplys for the ADS124S08. I am new to hardware design and I feel kind of lost with all the things I have to consider…
Part Number: LM27762 Other Parts Discussed in Thread: TPS745-Q1 , TPS62A01-Q1 , TPS628501-Q1 Tool/software: HI,
can you please suggest a regulator to generate +2.5 and -2.5V from 5V input? Output current requirement 100mA, with lowest possible drop…
Part Number: LM27762 Other Parts Discussed in Thread: ADS1120 Tool/software: I'm designing a PCB to power a sensitive analog sensor and read a differential analog signal (+/-10 mV) from the sensor. The input power to the PCB will be a noisy 5V, so I thought…
Part Number: LM27762 Hello,
I am using a LM27762DSST and noticed that the !PGOOD open drain output doesn’t seem to be capable of sinking very much current. I have a circuit that wants to sink about 3.4 mA through that !PGOOD node, but it looks like…
Part Number: LM27762 Tool/software: Dear e2e Support,
Do we have similar graph than the datasheet figure 5 to 8, with an input voltage of 2.7V and 3V? and ideally for a +/-5Vout.
Regards,
Part Number: LM27762 Hi,
I'm trying to understand the operation of the PGOOD pin on this device but I find the working of it confusing.
Within the Pin Functions it says that Logic 0 = Power good, Logic 1 = power not good. I assume that this means…
Part Number: LM27762 Hi,
We are planing to use this particular LDO in our project. I went through this thread where someone faced problems while using LM27762 , is this issue been solved? or is there any alternates that can be used for this?
Regards…
Part Number: LM27762 Hi team,
Datasheet merely shows "mV" for Output Voltage Ripple as below.
Just to make sure, does it mean mVpp(peak-to-peak)?
(Or Rms?)
Best regards,
Shota Mago
Part Number: LM27762 Hello team,
I am confused about the VOUT calculation equation. Which equation is correct?
On datasheet, the positive VOUT is VOUT = 1.2 V × (R1 + R2) / R2.
On the datasheet, negative VOUT is VOUT = –1.22 V × (R3 + R4) / R4…