Part Number: LM2901 One question about HBM. in the d/s it says it's +/-500V for non-B version. Does this device have related ESD rating for IEC61000 ESD/EFT?
Regards
Brian
Part Number: LM2901 Other Parts Discussed in Thread: TINA-TI
Hi , I am looking for LM2901 Ltspice Model for Simulation work Can you please Provide and we are planning to buy LM2901. Please reply ASAP.
Part Number: LM2901 Other Parts Discussed in Thread: LM339LV , Hi,
The customer finds a problem. When LM2901DR is supplied with 3.3V power, the output fails under -10 ° C in a low temperature environment. The waveform is as below, and the output failed…
Part Number: LM2901 Other Parts Discussed in Thread: LM339LV
Hi Experts:
Currently the project is planned to use LM2901DR as a comparator, if the supply voltage VCC provides a single +5V supply, IN+ is a fixed input of 0.5V reference voltage, and IN…
Part Number: LM2901 Hi team,
can the LM2901 (either B or non B version) withstand -1V from Vcc to GND (not to the input pins).
Datasheet seems to not give an absolute minimum, only the maximum voltage here.
Thanks!
Part Number: LM2901B-Q1 Other Parts Discussed in Thread: LM2901 , TLV1805-Q1 , TLV1704-Q1 , , LM339 Hi Experts:
It set VCC of LM2901 is 9~16V, IN+ =VCC/2 :
When IN- is equal to VCC-0.7V,is the out`pin output high?
When IN- is equal to 0V,is the…
Part Number: LM2901 Can you please provide p a) Minimum. b) nominal(typical), c) Maximum values of output saturation voltage curves with respect to output sink current (Io) over the temperature range. Datasheet provides output voltage saturation curves…
Part Number: LM2901 Dear Specislists,
My customer is evaluating LM2901D and has a question.
I would be grateful if you could advise.
---
In our circuit, Pin1 (1OUT) draws a large transient current (approximately 350ns) when switching from Hi-Z to Low…
Part Number: LM2901 Other Parts Discussed in Thread: TLV9032 , TLV3601 , TLV3201 , TLV3501 , TLV4376 Dear TI team,
I am using comparator IC LM2901PWR for 5A and -5A resonant current detection of bidirectional CLLLC converter. Resonant current will vary from…
Part Number: LM2901 Other Parts Discussed in Thread: , LM339LV Customer facing a noise issue and wondering to know what happened. pls see below description and schematic/waveform.
We found output of LM2901 is fault trigger (CH5) during noise coupling…