Part Number: LM2902-N Other Parts Discussed in Thread: LM2902 , , LM2902B Our procurement team indicated that this part will soon reach End-Of-Life. What's the latest order date?
Are drop-in replacements available?
Thanks,
Andy
Part Number: LM2902K Other Parts Discussed in Thread: LM2902-N , LM2902 , , LM2902B , LM224K , LM324K Is ESD the only difference between "LM2902-N" (PDIP package) and "LM2902KN" (PDIP package)?
Please let me know if there are any other…
Part Number: LM2902-N Other Parts Discussed in Thread: LM2902 Hi team,
My customer have a question regarding LM2902 ,
what situation or application of LM2902 circuit need to add dual common base-collector bias resistor transistors?
please kindly help…
Part Number: LM2902-N Other Parts Discussed in Thread: LM2902 , Hi,
I'm trying to compare LM2902 and LM2902-N components and I don't see much difference between them although the price per unit displayed on TI web site is quite different ($0.08 vs $0.35…
Part Number: LM2902-N Other Parts Discussed in Thread: TINA-TI , LM2902 I'm designing a voltage to high side current current source converter. To check stability, I have broken the loop and measure the loop margin. With R3=2k, C2=1n and R2=4k the phase…
Part Number: LM324A Other Parts Discussed in Thread: LM324-N , LM324 , LM2902KAV , LM2902K , LM324K , LM2902 I have an old PCB that I am updating so that it will pass the 15kV air discharge test. It is using the LM324N, and LM324AN interchangeably as voltage…
Other Parts Discussed in Thread: LM358 , LM2902 , LM324 , LM2904 , LM358-N , LMV324 Hi,
Let me ask you a basic question about LM358 application circuit as below.
Is a load resister like "Rb" (6.2K ohm) necessary to use LM358?
What is the purpose of…
Hello Binoy,
FWIW: The LM2902 *is* a LM324 - same die...just tested to different parameters. The LM358 is the dual version of the LM324...same circuit. The LM741 is not suitable for single supply, ground-referenced circuits.
But at 3.3V supply, the maximum…
To reiterate what Art said, the LM324 is not a good choice for low distortion applications.
The LM324 was originally designed for true single supply applications, with the load returned to V- ("GND" pin). The LM324 has a "unique" output stage that requires…