Part Number: LM2903-Q1 Hi,
My client requested a schematic review.
OUTPUT1 : 4.5V High
OUTPUT2 : 1.2V High
The purpose is to output the low output of the final PWM_EN stage.
Please review the schematic.
Hi Shunsuke-san,
Since both channels are on the same die, exceeding the absolute maximum input current on one channel has the potential to destroy the entire device (both channel 1 and channel 2) due to electrical overstress. It's a possibility that only…
Part Number: LM2903 Other Parts Discussed in Thread: TINA-TI , , LM339 , Hello,
We are going to use this IC as Schmit trigger comparator.
As this is open collector, what will be the output response (Logic High/Low) if +ve input is more than -ve input?
Any…
Part Number: LM2903-Q1 Hi team,
My customer highlight LM2903-Q1 part number issue.
In their factory system, they saw LM2903QPWRRB part number but in TI system, we can't see this part number.
So we need BU to clarify the reason and give customer's…
Part Number: LM2903 Hello,
We need your help to identify the difference in part numbers-LM2903DR, LM2903VQDR, LM2903QD. Are this MPNs compatible to each other.
We appreciate your soonest response.
Thanks & Regards
Pratiksha Walunj
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903B , LM339 , TLV1811 Why the red circled part are 10M and the other resistors are 10k, if we change the 10M to 10k, what will happen and why?
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM339 The comparator is powered by dual power supplies, and after a problem with the negative power supply, the comparator output is abnormal, can you help explain how the negative voltage power supply…
Part Number: LM2903 Hi
There are differences in marking font format, and there are also slight differences in the material plates. Some material plates are of two colors, while others are of one color. Could you please help confirm the reason
Thank y…