Part Number: LM2903-Q1 Hi team,
My customer highlight LM2903-Q1 part number issue.
In their factory system, they saw LM2903QPWRRB part number but in TI system, we can't see this part number.
So we need BU to clarify the reason and give customer's…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM339 , LM2903 , , LM2903B Hello TI,
Where can i find input leakage current of LM2903-Q1 . I could not find it in the datasheet. Kindly provide input leakage current of both inputs and its variation with…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM339 The comparator is powered by dual power supplies, and after a problem with the negative power supply, the comparator output is abnormal, can you help explain how the negative voltage power supply…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903B , LM339 , TLV1811 Why the red circled part are 10M and the other resistors are 10k, if we change the 10M to 10k, what will happen and why?
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903 , LM339 , LM2903B-Q1 , LM2903B Hi team,
My customer is using LM2903-Q1 in their traction inverter system. During the inverter switching there will be noise coupling to the input pin, making the…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903B-Q1 , Hi team,
I searched datasheet that those PNs different is Device Marking. will it affect the function or application?
BR,
Jimmy
Part Number: LM2903-Q1 Hi, Team
Hope you are doing well!
For LM2903-Q1 family, I have two questions:
Q1: Which category does LM2903VQPWRG4Q1 belong to in the following table?
Q2: What are the part number corresponding to "A" Devices and "AV" Devices?…
Part Number: LM2903-Q1 Hi team,
Could you pls help clarify, if customer V+ is 12V (within 36V rating), IN- is below (V+ )-1.5V, can IN+ go up to beyond (V+ )-1.5v, eg 18V? Device still functions normally in this case, right?
Thanks
Scarlett
Part Number: LM2903-Q1 Hello Team,
What is the sinking current of LM2903-Q1 IC??
Shall i consider sink current is same as output current??
Regards,
Giridhar.