Part Number: LM2936 Could you please confirm that LM2936BM is intended to work with Pin 5 left open? Customer is switching from LM2936BM to LM2936M. Do they need to expect any issues?
Regards
Andreas
Hi Nick,
1.
yes, I have put a series resistor + ceramic capacitor as an option into my layout.
2.
Yes, this was one part of my question. the other part was about the thermal pads that you can see (marked with yellow pencil) in my screenshot (from February…
Part Number: LM2936 Hi There! There is stock online of LM2936 C M-5.0 at Rochester Electronics (see picture and link) but I can't find this to be a valid part number anywhere. Can you advise what the C denotes and if this is a valid PN? Thanks! Kara
…
Part Number: LM2936 Hi there,
Regarding the LM2936QM-5.0/NOPB, may I ask why the colors of the holes in the same tube in the same box of a batch are different, some of which are bright and some are dark, is this normal?
Part Number: LM2936 Hi Team,
Good day! Could you please help us to find the meaing of suffix "A" for LM2936HVMA?
Thank you so much.
Best regards,
Jonathan
Part Number: LM2936 Hi Team,
Our customer is using our voltage regulator LM2936 to generate 3.3Vout however, they only used a 10uF ceramic cap instead of the recommended 22uf for Cout from the datasheet.
The customer claims that they had no stability issue…
Hello Archie,
If the capacitors (say 'N' of them) connected in parallel have identical capacitance (C) and ESR (R ESR ) values, only then will the equivalent capacitance (C EQ ) and ESR (ESR EQ ) be easy to calculate (C EQ = N*C & ERS EQ …
Part Number: LM2936 Hi,
We are using LM2936QDT-5.0/NOPB in one of our projects. We are yet to receive our PCB with this part. Meanwhile want to check my calculation of PCB temperature while subjecting the device to output short circuit condition.
…
Part Number: LM2936 Hi TI Expert I have an over heat problem in LM2936MP-5.0 When the external power is 30 V.
The load current is below 30 mA.
Regards
Ihab