Part Number: LM293A Hi team,
I cannot find LM293ADGKR's package(VSSOP) information in datasheet, could you please check if its package is compatible with INA296A1IDGKR? Thanks!
Nison
Part Number: LM293A Other Parts Discussed in Thread: LM193 , LM393 , LM293 Dear Specialists,
My customer is considering LM293A and has a request.
I would be grateful if you could advise.
---
Datasheet P.11 Figure 6-3 shows the output characteristics when…
Part Number: LM293A Other Parts Discussed in Thread: LM293 , Hi There,
Please see attached image of LM293 used as comparator to monitor +24VDC supply. I am bit doubtful about the hysteresis provided as the reference is on inverting input. Can you please…
Part Number: LM293A Other Parts Discussed in Thread: LM293 , LM2903B Questions about the comparator LM293ADR, please help to answer. 1. There are two test conditions for response time in the specification. What is the main difference? Why is the time difference…
Part Number: LM293A Other Parts Discussed in Thread: LM393B , LM339 Hi Teams
Customer selected LM293A in their new project for overcurrent protection but they found the respond time is slow than datasheet spec.
The schematic have shown below. We measure…
Part Number: LM293 I saw someone use one series RC cross positive input and output of LM293. Usually, it composes an integral circuit if RC is cross the negative input and output of one OPA. However, I do not know why the similar circuit is used in comparator…
Part Number: LM293A Hi team,
customer use LM293ADR as over current protection, but have a problem is that the set over current value is 25.9A, but when the current is only 20.4A, the LM293ADR will output high from low. the schematic as below:
They use…
Part Number: LM293A Hi,
Can you please confirm whether the max supply current spec in the datasheet of 1mA is for the two channel or per channel?
-Kelvin
Part Number: LM293A Hi all:
Have a reply:"The first stage, U5A, is at the biggest risk. Both the input and reference voltage exceed the limit and has the possibility of an incorrect output."
However, IN my actual test, the voltage of U5A IN…