Part Number: LM3100 Tool/software: Hi, team
We have a GaN opportunity in 48V EPS, and customer are evaluating the overCurrent Capability and Power Dissipation under 10k~100Khz f_sw.
Do we have a test data to support it? Or any evaluation guideline…
Part Number: LM3100
I am using one of your product LM3100MHX/NOPB
I have a doubt about designing the feedback resistor rfb1 and rfb2 for 5v from a input of 24v
in the datasheet it says to choose the value…
Part Number: LM3100 Hi,
I'm trying to calulate the inductor (L) value for my LM3100 regulators. I'm running into an issue with Equation 11 on p. 13 of the spec sheet. It refers to using Equation 1 to get the switching frequency (Fsw). However, Equation…
Part Number: LM3100 Hi,
I have a customer who wants to work with the LM3100 as a load switch protected from reverse polarity with very low off current.
He wants to disable the use of the UVLO function.
Can he connect it to GND so it won’t take power…
Other Parts Discussed in Thread: LM3100 We are using a TI power supply for another project of ours (LM3100).
http://www.ti.com/lit/ds/symlink/lm3100.pdf
On page 3 it states:
"(2) If Military/Aerospace specified devices are required, please contact…
Other Parts Discussed in Thread: LM3100 7612.SCHEMATIC _ Main Board Rev B - Page 2.pdf
We are having a problem with a LM3100 in that the output voltage is not constant as the load varies. The output is stable with very little switching noise, but goes…
Other Parts Discussed in Thread: LM3100 , LMR24220 We use the LM3100 for dc/dc conversion from 24 V to 5 V (see schematic, calculated output voltage: 0.8 V*(1+6.81/(2.61/2)=4.975 V). It works, but the output voltage is not as constant as told in the data…
Other Parts Discussed in Thread: LM3100 I have a question for LM3100 electrical characteristics.
1.Current Limit Min, Max Value.
2.Enable pin input current.
3.ON timer pulse width Min, Max Value. under Ron=200k,Vin=24V,Vo=5V
Other Parts Discussed in Thread: LM3100
Hello,
One of my customers needs the following information on LM3100 part:
When
simulating LM3100 using Webbench , there are no bode plot simulation is available.
Please address the following…
Part Number: LM25085 Other Parts Discussed in Thread: LM3102 , LM25011 , LM3100 Hi, I have an urgent issue about the LM25085:
Circuit Description: LM25085, as the first-stage Buck chip, is connected to the supercapacitor through the MOS driven by the…