Part Number: LM3102 Hello,
The datasheet specifies only Icl for typical value:
What is the maximum value of this current limit threshold?
Hoping someone from TI could respond to my question.
Part Number: LM3102 Hy,
is it possible to change the value of the output voltage in dependency of the SS-Voltage ?
For example, if I use a DAC to manipulate the voltage between 0V up to 1V ?
Kind regards
Part Number: LM3102 Other Parts Discussed in Thread: LM20242 Hi Ti,
I am facing light load regulation issues with LM3102 - output voltage 12.5V, input voltage from range 15-30V. Voltage goes up to 14V at the DCM condition, IC feedback is not reacting…
Part Number: LM3102 I purchased the LM3102TL-1-NOPB but the datasheet claims the DSBGA package has a reduced current output. Does that mean that part can't output 2.5A?
Part Number: LM3102 Designing a new power step down voltage regulator.
We need a very low noise 5-volt power supply, approx. 20 - 30 uVrms
Input 12 volt (stable) max 2,5A, operating temp range approx. 30ºC 40ºC
I tried to find a regulator in the…
Hello,
In the datasheet, Cvcc is recommended (One place says "should", another says "must"??) to be no smaller than 680nF. I have a nitpick clarification question so as to avoid potentially overdoing that capacitor. Is this datasheet stating that the…
Hello,
It is basically that for outputs above 7V, the operation cannot be guaranteed. The internal parameters are designed for optimal performance for outputs below 7V.
Regards,
Akshay
Other Parts Discussed in Thread: LM3102 Hello,
I have a project that uses LM3102 converter, we have ordered about 25 chips in TTSOP package for prototypes batch and have found an interesting issue.
It seems that for some of the chips pin 7 (AGND)…