Part Number: LM311-N Other Parts Discussed in Thread: LM311 , TLV1812-Q1 Hello guys,
One of my customers is considering using LM311M(X)/NOPB. They have the following questions. Could you please tell me your reply?
Q1. What is LM311-N minimum operation v…
Part Number: LM311-N Have been using Capture CIS 17.4 for a few months now and have been using components from the Cadence standard library. I've just started using Pspice for TI and I gather looking at other threads that trying to simulate a circuit…
Part Number: LM311 Other Parts Discussed in Thread: , LM6511 , LM211 Hi team,
What is the difference between LM311, LM311-N and LM311-M?
I can't see big difference between them on the internal circuit in the DS.
I would like to use it for GND standard…
Part Number: LM311-N Other Parts Discussed in Thread: LM393-N , LM311 , TL331 , LM339 , LM393 I'm using the LM311N/LM211P in a basic zero crossing detector circuit as in Fig 13. below with a pull-up voltage divider to give 3.3V logic output. The attached…
Part Number: LM6511 Other Parts Discussed in Thread: LM319-N , LM311 , LM306 Hello
I Would like to Desigh Zero Crossing detector Using LM6511 or LM319. Input is 100kHz Inverter current from a Resonant mode Controller.. I Simulated using LM6511, But SPICE…
Part Number: LM311-N Hi,
Our customer keeps using "LM311H/NOPB" but I cannot find the data sheet on TI website, so could you please share it with me ?
Best regards, Kato
Part Number: LM311-N Other Parts Discussed in Thread: LM311 , LM7705 , LM6511 , LMV7235 Using this comparator LM311 based on the attached schematics, only when the reference voltage at the inverting input is above 78mV does the output signal voltage pull…
Part Number: LM193-N Other Parts Discussed in Thread: LM193 , TLV3201 , TLV2371 , LM311 , LM111 , SN6505B , OPA381 Please explain the following circuits. Why are resistors chosen the way they are chosen? one of the circuit has a pull-up and the other doesn't…
Hello Keith,
The balance pins are connected to the emitter resistors in the front end diff pair.
The balance pot is placed across these pins and adjusted to slightly change the tail currents to correct the offset voltage by a few mV.
It would be possible…