Part Number: LM317A Hi team,
My customer wants to use LM317A to convert 5V to 1.275. The schematic is as below. But the output voltage is wrong(3.1V) at light load.
Do you have some ideas?
Part Number: LM317A-337N-EVM Other Parts Discussed in Thread: LM317A Are the physical dimensions of the LM317A-337N-EVM board mechanical features available? They are not included in the User's Guide. I need the minimum required for mechanical accommodation…
Part Number: LM317A According to the datasheet, the capacitors are recommended to be tantalum.
For example, on page 12 of the datasheet, the authors suggest using a disc or a tantalum capacitor, "An input-bypass capacitor is recommended. A 0.1-μF disc…
Part Number: LM317A Other Parts Discussed in Thread: LM317 Hello,
We are considering using LM317A for an application that require good Vout accuracy of 2.5% over time and in temperature.
Our application is 30V -> 24V with very small Vin range and Vout…
Part Number: LM317A-337N-EVM Other Parts Discussed in Thread: LM317 , LM337 Hello,
I am designing a Gate Driver with configuration Plus and Minus Gate voltages for SiC Mosfets. The Plus one shall range from +9V to +18V and the minus one from 0V to -12V…
Part Number: LM317A
Hi teams,
I have a customer that design in LM317A and they want to know the case temperature.
The customer using TO-220 package and have a case over heat issue.
And they are wondering if they can know the case temperature by the information…
Part Number: LM317A Hi support team, I have a question about the link of the LM317A datasheet.
Is SLVS044Y link incorrect?
www.ti.com/.../lm317.pdf
Is it correct SNVSAC2A? www.ti.com/.../lm317a.pdf
Regards, Dice-K
Part Number: LM317A Other Parts Discussed in Thread: LM317
Dear sirs,
I am using the LM317A to have 37V at the output side with 48V at the input side. This should be possible according the specific regarding the input output maximum difference voltage…