Part Number: LM317L Hello Team,
I have an urgent request about LM317L
Could you address this subject ?
The other company has a description of thermal resistance with the following figure.
Can we provide same figure ?
Any advice will…
Part Number: LM317L Other Parts Discussed in Thread: TPS2553 , LM317 Dear Sir,
Please check the datasheet page 12 "9.3.6 50-mA Constant-Current Battery-Charger Circuit".
I want to use the current regulator to limit the input current.
My resistor…
Part Number: LM317L-N The package hast 6 pads, but only 3 are used.
The "NC / No connection" pins, can they be used for routing? Or should they be left floating?
Best regards
Sebastian
Part Number: LM317L Other Parts Discussed in Thread: LM317 Hi,
We are charging a 2200mAh battery with the LM317L . Please see the attached schematics of the implementation. The input supply is 12V and the output voltage adjusted to 11V. Please advice…
Part Number: LM317L
“Minimum Output Current to maintain regulation” shows as below. Its condition: Vi-Vo=35V (Beyond the recommended operating condition).
In usual case…..Differential voltage 2.5V to 32V doesn’t have minimum output current restriction…
Part Number: LM317L Hi Team,
My customer would like to know if we can provide the thermal resistance of LM317LIPK.
1) Thermal Resistance (Junction to case) (top) °C/W 2) Thermal resistance (Junction to ambient) °C/W 3) Thermal resistance (Junction…
Part Number: LM317L Other Parts Discussed in Thread: LM317 , , LM317A Hi, Team.
This is MASA.
Could you answer for below the question my customer asked me?
Q1. In the datasheet shows that "output regulation" is 0.5%.
Q2. what does "reference…
Part Number: LM317L-N Hello Team.
I would like to confirm the behavior at short circuit condition.
Could you let me know how the over Temp & over current protection work ? (1) Specifically, the detailed behavior at Over temp, the release threshold…
Part Number: LM317L-N Hello, We have a customer with a military application, looking for the LM317L-N in a leaded version (not lead free), needs an 8 pin SOIC package. Do we have any device options for him? Thanks,
Part Number: LM317L-N Can you confirm if the connections to the TO-92 package are seen from the bottom or top?
The datasheet on page 3 shows ‘bottom view’ below the device and ‘top view’ above the4 device – which one is correct?