Part Number: LM339 Other Parts Discussed in Thread: TLV9024 Hi Team,
Do we have Pin2Pin device with LM339 but response time less than 0.1us? Thanks.
BRs,
Francis
Part Number: LM339 Hi,
I want to confirm whether the high level output current is for each channel or the total current, which is not specified in the document.
Many thanks~
Part Number: LM339
Hi Experts,
Kindly assist us with this query.
From the application note, I got that information in Figure 13 includes a circuit to detect full charge and gives a visual indication of charge completion with an LED. This circuit turns…
Part Number: LM339 Other Parts Discussed in Thread: LMV339 , , TLV1702 , LM393B , TLV9024 , LM2903B , TLV7044 Hey!
Are there any comparators similar to the LM339 which come in a QFN package? I did an unfruitful parametric search (likely because I’m on mobile…
Part Number: LM339 Other Parts Discussed in Thread: LMV331 , , TL331 , LM393 Hi there,
say i have a quadruple comparator with FIT rating 2.2 like the LM399 (A generic single one like the LMV331 has a FIT rating of 11.6).We have now the following discuss…
Part Number: LM339 Good Day
The Ti LM339 application note states that inputs should not be connected directly to a low impedance node. In my case does this mean Version A of the circuit is the correct one? The only difference between the two is the 1k…
Part Number: LM339 Hi TI team, merry christmas and happy new year!!
I am using a LM339 comparator to detect a LED circuit.
The input from LED circuit is 5V or 3V.
I hope when input is 3V, LM339 output low and MOSFET on.
and when input is 5V, LM339 output…
Part Number: LM339 Other Parts Discussed in Thread: , TLV1704 Team,
can you help explain why we get 0.79V on the output regardless of input in this schematic?
Part Number: LM339 Other Parts Discussed in Thread: LM139 , LM239A , LM239-N , LM2901-N , LM2901V , LM2901 , LM239 Hi,
we wanna use the LM339 in our design. The junction temperature of this device is quite limited and we wondering if the Tjmin (0degC) and Tjmax…