Part Number: LM34 Tool/software: Hi engineer
can you help me ? we purchased 1000pcs from TI store. test 1000pcs, 6 pcs indicated low resistance.
Issue: Failed resistance test - Low resistance Specification: 65 to 85 kohms
Failure Analysis: 1) Replaced…
Part Number: LM34 Tool/software: Hi team,
I want to confirm with you what is the package for the item LM34AH.
it this in bulk? tray? tube? please help me to confirm.
Part Number: LM34 Hello, I am looking for information on the actual sensing region of this probe: LM34AH silicon based temperature sensor. Is the temperature averaged over the entire 5mm diameter top surface? Or is there a smaller sensing region within…
Part Number: LM34 Hello,
We are located in India whom constantly involved in procurement of "LM34DZ/NOPB" for 1000/2000 Pcs in a Single Ordering.
Currently we have found out that these parts are out of stock and No information on when these will…
Part Number: LM34 We have been using a LM34 for the past 30 years as a temperature sensor in a device we manufacture. We have not had any issues until recently. The issue is that 1-2% of the sensors will work fine then swing widely from low to high and…
Part Number: LM34 Hello, dear colleagues.I'm sorry, I couldn't specify the correct part number in the form, it is written that such a part number was not found. So I specified a similar one. Please help me understand the markings on the bottom of the…
Part Number: LM34 Hi,
I am looking into a temperature sensor for a future project. I see that the LM34 states that it has a maximum supply voltage of -0.2V. Is this correct?
Thanks
The LM34 plus connected to +5 volts. Minus is connected to ground and Vout is connected to a microchip pic AtoD pin unless something is wrong using a Pic?
Part Number: LM34
Hello, customer order the LM34DZ/T7 in the past and wants to use the LM34DZ/LFT7 now. Are these the same parts? Is the LM34DZ/T7 obsolete? Is there an obsoletion letter?
Regards, Holger