Part Number: LM3492AR111DEMO
Hi,
Can anyone explain the current limit circuitry? Why the LED current is set at 360mA but from what i measured the LED current is limit at around 200mA.
What is the purpose of the peak current limit circuitry?
Regards…
Part Number: LM3492AR111DEMO Other Parts Discussed in Thread: LM3492 , TPS92560 Hello ,
I am designing a luminaire using LM3492 to drive four strings of duris S5 white LEDs ( LED VF is 6.1V and IF is 125mA). Currently i'm implement the configure 4S4P to…
Hi Irwan,
Our application are need three type of input voltage such as 12VAC, 24VAC and 32VAC. We are looking a solution can power up with three type of the input voltage and can get a better power factor and efficiency. Currently we are using LM3492…