Part Number: CDCE6214-Q1 Is there a ready reference to the capabilities of the device using EEPROM default pages on startup?
My work environment does not allow the loading of software that might allow me to review the effects of various presets.
Thank…
Part Number: USB2GPIO-LOADER-SW Other Parts Discussed in Thread: USB2ANY I installed USB2ANY explorer from TI SDK. I changed my interfaces to I2C. I'm not able to see I2C option popping up( I tried in my friends laptop, it worked. There are few options…
Part Number: TICSPRO-SW Other Parts Discussed in Thread: USB2ANY Hi Experts,
Asking your assistance on this query about TICSPRO-SW. For this tool, can we use a USB to I2C adapter other than a USBTOANY adapter? Customer has Aadvark adapter to use USB to…
Part Number: LM3549 Dear Sir/Ms.
How much time has passed after Power on can I2C Command be given to LM3549? How much time has passed after R/G/B Enablae can I2C Command be sent to LM3549? My customer used the polling method to issue I2C commands, and then…
Part Number: SW-EK-LM4F120XL Other Parts Discussed in Thread: EK-TM4C123GXL I have made a function in order to configure I2C communication from an LM4F120H5QR microcontroller with an external sensor (HMC5883L).
I have used register definitions from lm4f120h5qr…
Part Number: MSP430FR2111
Customer is debugging 100 kHz I2C Slave connecting to a host from SW_I2C_ slaa703a.pdf app note/code.
>>With 8-MHz MCLK , software slave I2C can achieve 100-kHz SCL clock frequency using assembly code and 43-kHz SCL clock…
Part Number: TICSPRO-SW Other Parts Discussed in Thread: LMK03328 Hello,
As the title suggests, is there a way find all the devices on an I2C bus? I am using the LMK03328 for a test board, and have multiple devices on that I2C line. Right now it looks…
Part Number: LM3549 Hi Team,
below are several questions on LM3549
1. for brightness control, if just use I2C register, then can PWM pin be floating? we can ignore the PWM input signal at this time, right?
2. is there power sequence requirement between…
Part Number: SW-EK-TM4C129EXL I have searched all through these forums and not found any answers that have helped so far.
I am using TI-RTOS 2.16_01_14 with TivaWare 2.1.1.71b. It seems that my calls to the I2C API functions are hit or miss for whether…
Part Number: LMK03318 Other Parts Discussed in Thread: USB2ANY Hi
I would like to know if I can configure my on board PLL via the TICS Pro SW and USB to I2C Elite programmer
( https://i2ctools.com/product/usb-to-i2c-elite/ )
Regards
Omer