Part Number: LM36010 Hi Team,
could you please kindly help test eff @ 100mA similar as below curve ( different Vin) ?
my customer want to know if peak eff can meet 85% @ 25C, 80% @85C. Thanks.
BRs
Given
Part Number: LM36010 Hi Team,
just want to check if eff curve in datasheet already conclude eff @ pass mode . Since it is tested at VLED = 3.4V and Vin changes from 2.5V to 5.5V, so there is pass mode, right? Thanks,
BRs
Given
Part Number: LM36010 Hi,
In the datasheet, the Figure 35 is for writing. Does LM36010 support reading of the registers? Does it support re-start?
Thanks.
Part Number: LM36010 Hi team,
My customer is not clear with the name "IR mode".
Do the customer have to use the IR mode when lighting a IR LED?
Or is it only a mode that is recommended for IR LED usage?
In addition,
I guess that LM36010's…
Part Number: LM36010 Other Parts Discussed in Thread: LM3644 , LM3648 Hi team,
My customer wants to use 5V input to drive one channel 5 LEDs in series. The total voltage drop of the 5 LEDs in series is about 7~8V. So customer wants to find a boost structure…
Part Number: LM36010 Hi, team
Level trigger and edge trigger.
I test on EVM, in level trigger, LED turn off when STORBE go to low; In edge trigger, LED turn off when SOTRBE go to low and and after flash time out.
Is this the only difference level and…
Part Number: LM36010 From my customer-
I have designed a circuit for LCD backlight as below screenshot, and we have some problem.
We would like to control the current for LCD backlight from 0mA to 120mA, but we cannot increase the current over 55mA. …
Part Number: LM36010 Other Parts Discussed in Thread: LM36011 Hi E2E,
Good day!
Is it possible to implement an inductorless or simplified configuration using LM36010?
Looking forward to your response.
Best regards,
Franz