Part Number: LM385-1.2-N To whom it may concern,
Please let us know what is the difference between the following products.
・LM385BZ-1.2/NOPB
・LM385B X Z-1.2/NOPB
What does the X in the model number indicate?
We initially thought that X indicated the package…
Part Number: LM385-1.2 Hi,
We are using the LM385MX-1.2 SOIC8 Package in few of our designs.
I would like to help us with the below query..
What's the difference between
1. LM385M-1.2/NOPB
2. LM385M-1.2
3. LM385MX-1.2/NOPB
Is any of the above made…
Part Number: LM385-1.2-N
Hi There,
I have a design that utilizes the LM385Z-1.2/NOPB Voltage reference IC. I know that the temperature specification for this part is 0-70C in the data sheet. I want to know how this component will operate at temperatures…
Part Number: LM385-1.2 Hi team,
My customer wants to use LM385-1.2 but use the FORMED LEAD OPTION. But I cannot tell which part number refers to the FORMED LEAD OPTION instead of STRAIGHT LEAD OPTION. So could you please help share the full part number…
Part Number: LM385-1.2 Hey Team,
I have a customer that is using the LM385 (I don't know full part number) for their previous generation handheld Digital Multimeter.
Could you provide any recommendations for a device that targets higher precision…
Part Number: LM385-1.2 Hello All,
My customer is using LM385-1.2 in package SOT-23.
They are now looking for the same product same package with temperature range -40°C +100°C, any comments here?
Many Thanks,
Antonio
Part Number: LM385-1.2-N Hello all,
For the LM336-2.5N and LM385-1.2-N packages can you verify if the pins start from( left to right 1 2 3) or (right to left 3 2 1)
The package outline drawing is a little confusing, link below:
http://www.ti.com/lit/ml…