Part Number: LM3880-Q1 Hi Team,
Could you please kindly help to check what is the difference between -1AA; -1AB;-1AC;-1AD;-1AE;-1AF? Thanks a lot for your support to confirm.
Best regards
Jie
Part Number: LM3880-Q1 What is the minimum EN low time needed to ensure that the power up sequence is done with the proper timing? In other words, if I have a 10 ms sequence 1 device (timing designator AA) and EN is low for 30 ms to ensure a normal power…
Part Number: LM3880-Q1 Other Parts Discussed in Thread: LM3880 Hello team,
My customer wants to decrease quiescent current at standby situation for LM3880-Q1.
LM3880-Q1 output should be 'L' at standby.
So, The current is needed not only LM3880…
Part Number: LM3880-Q1 Team,
Is the LM3880QMF-1AE/NOPB logic bearing?
I believe the reason for this question is because if it is programmable then there is a supply chain risk that my customer needs to manage/mitigate.
Thank you.
Part Number: LM3880-Q1 Hi Sirs,
Sorry to bother you.
Could you help provide LM3880QMFE-1AE/NOPB ESD CDM value for us ?
Thanks!!
ESD-HBM :
ESD-MM :
ESD-CDM :
ESD Report or Evidence (Y/N) :
Pass/Fail :
Hi Travis,
I am not sure I understand "you have to sink current from the EN pin to ground to stop it from turning itself on." 1) could you tell me the way I could do it ? 2) actually, R166 ties low EN pin when Q1 does not conduct. 3) I have physically…
Part Number: LM3880-Q1 Other Parts Discussed in Thread: LM3880 Q1. Customers use the LM3880-Q1 in cascade. *For the circuit configuration, refer to the attached file "circuit diagram".
When EN changes like attached file, 1)LM3880-Q1 Sequence-…
Part Number: LM3880-Q1 Other Parts Discussed in Thread: LM3880 I would like to confirm the power down sequence of the LM3880-Q1.
It is described on page 11(7.3.2 Incomplete Sequence Operation) of the LM3880-Q1 datasheet as follows.
------------------…
Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: LM3880 , TPS22993 Hi Team,
Can you suggest a power management module that would allow the user to enter/exit the sleep mode feature of the phy ethernet DP83TG720S-Q1?
Can you confirm the combination…
Part Number: LM3880-Q1 Other Parts Discussed in Thread: LM3880 ,
Hello,
Please answer following request from customer.
Following Applications Journal Figure 4 explains the example of LM3880 cascading circuit.
http://www.ti.com/lit/an/slyt598/slyt598…