Part Number: LM4132 Other Parts Discussed in Thread: REF4132 Hello,
Could you please provide CDM of ESD ratings for the LM4132?
I could only find HBM information in the datasheet as shown below.
Thank you.
JH
Part Number: TMS570LS3137-EP Other Parts Discussed in Thread: TMS570LS3137 , LM4132 , HALCOGEN HI TI team,
We are planning to operate (ON/OFF) LM4132-2.5V Reference IC by using GPIO port B of TMS570LS3137.
LM4132 input voltage is 5V and EN pin is pulled…
Part Number: LM4132 Other Parts Discussed in Thread: REF4132 Pin 1 of the LM4132 is labeled 'no connect pin'. Is it a problem if I connect the pin to FND?
Part Number: LM4132 Using the 2.5V reference the output is 2.85V (14% error) with 5.05Vinput and Cin=Cout and 20k Ohms load. If I remove the 20k Ohm load the Vref output measures 4.4V. The EN pin is pulled up to Vin through a zero Ohm jumper. What is…
Part Number: LM4132 Other Parts Discussed in Thread: REF35 , REF4132 , Hi
I have a high speed adc design(ADC 3669) which requires the reference voltage of 1.15 for which i followed a approach from one of high speed adc EVK as below
kindly let me know…
Part Number: LM4132 Hi, Good day. I hope you are doing well. Our customer has this inquiry about the LM4132. Can you please help us? Thank you. We have implemented the LM4132DMF-3V3 in a new design. The part supplies 3.3V rail to a TCXO. We have measured…
Part Number: LM4132-Q1 Other Parts Discussed in Thread: LM4132 , TPS62180 , TPS62147 , LM5176 , TPS54326 , TPS2065 , TPS51362 , TPS548A20 , TPS65177A , LM3643 , TPS62175
Hi Team,
Our customer would like to confirm if the devices below are multi-component semiconductor…
Part Number: LM4132-Q1 Hi team,
My customer asked me the maximum voltage at VREF pin when disable.
Does your team have such a data? I think VREF pin becomes Hi-Z, not low. So, I think there is no such a data. But, I appreciate if you could check if you…
Part Number: LM4132 Other Parts Discussed in Thread: REF4132 Hi,
I'm looking for LM4132 Spice model.
But I couldn't find it out.
I want to simulate Transient response with input voltage fluctuation.
I want you to provide the model, or alternative…
Part Number: LM4132
Hello,
My customer is using LM4132BMFX-3.3/NOPB for Vin=5V and Vout/Iout=3.3V/15mA as follows.
edit:removed schematic
The following is the startup waveforms of IN and VREF.
VREF has some overshoot.
Any suggestions to prevent this…