Part Number: LM43602 Hi,
I use DCDC LM43602 and have next have DCDC Requirements:
1. Very wide Vin – from 5.5V to 29.3V
2. Output Current – min 30mA to max. 800mA
3. Vout is 4.37V
I used TI Webench
And, calculated by formulas from Datasheet…
Part Number: LM43602 Could you please let me know status about this question?
---
Question of PFAS and C9-C14 PFCAs
Reagrding following's 2 substance groups. We have received the following requests from our customers. Can the following TI products meet…
Part Number: LM43601
Team,
a)Assuming that you have an existing PCB validated with LM4360 1 PWPR (max Iout 1A). Can it be replaced by LM4360 2 QPWPRQ1 or LM4360 2A QPWPRQ1 (max Iout 2A): -without any changes in the schematics (ie change of passive around it…
Part Number: LM43602 Reagrding following's 2 substance groups. We have received the following requests from our customers. Can the following TI products meet this requirement?
(1)PFAS (Per- and polyfluoroalkylsubstances) <Threshold level> Not intentionally…
Part Number: LM43602-Q1 Other Parts Discussed in Thread: LM63625-Q1 Dear TI,
Does LM43602-Q1 support asil b iso26262 or do we have similar device that can support asil b iso26262? Thanks.
Part Number: LM43602 Other Parts Discussed in Thread: LM76002 Hi! I am currently designing a LM43602DSUR regulation circuit, with the following parameters:
Vin = 24 V
Vout = 1.2 V
Iout = ~2A
My original plan was to use the default switching frequency…
Part Number: LM43602 Hello,
I have a question about FB resistor selection. The datasheet recommends RFBB=43.2kohm when Vout is 24V. (RFBB is connected FB to GND.) Is it possible to choose RFBB=4.32kohm instead? I wonder if there is any problem on the device…