Part Number: LM43603 Hello guys,
One of my customers is considering using LM43603 for their next products. They are simulating LM43603 with Webench. At this moment, they have the following questions. Could you please give me your answer to the questions…
Part Number: LM43603 Other Parts Discussed in Thread: LM61440-Q1 Just received word that there can be some inrush issues if there isn't some matter of "slow start" for the LM43603 converter. It takes some time 't' to rise for a soft/slow start, but there…
Part Number: LM43603 Hi teams,
My customer want to pull up PGOOD pin to VCC pin.
Is that OK?
Regarding to the datasheet, It doesn't allow VCC pin to connect any load.
Thanks,
Shoo
Part Number: LM43603-Q1 Other Parts Discussed in Thread: LM43603 , LM46002 We are having startup issue with using an LM43603 rather than a LM46002. Schematic below.
When the supply has around 6V to 8V at the input the output ripple is around 400mV. When…
Part Number: LM43603
I have made 2 PCBs with the same schematic shown but different layouts. One circuit works fine and the other has poor output voltage regulation.
On the one that has poor regulation, under no-load it outputs the desired voltgae (5…
Part Number: LM43603-Q1 Other Parts Discussed in Thread: LM43603 Hi Team, The datasheet shows the following. --------------------------------------------- LM43603A-Q1 version is optimized for PFM operation and recommended for new design. The device is pinto…
Part Number: LM43603-Q1 Dear TI
I am thinking of replacing "LM43603PWPR" with "LM43603AQPWPTQ1".
Please answer the following two points.
(1) "LM43603AQPWPTQ1" is an in-vehicle grade product of "LM43603PWPR", and can it be considered…
Part Number: LM43603 Hi TI Team,
I would like to check if this part is able to undergo the washing process (using DI water).
Please provide any relevant supporting document if possible.
LM43603DSUR
Thanks.