Part Number: LM46001 Hello,
My customer is considering to use LM46001.
But because they couldn’t find any available samples for LM46001, they got LM46001-Q1(non-A version) samples instead for their 1 st prototype.
Could you tell me the difference…
Part Number: LM46001-Q1 Other Parts Discussed in Thread: LMZ34002 , LM46002-Q1 , LMZM23601 , TPSM5601R5H , LMZ14201H
Hi,
i was looking for a 18v-36v dc input to +-15v dc 1A output buck converter.
i came across the device LM46001-Q1 which has a reference…
Part Number: LM46001-Q1 Hi Team,
LM46001-Q1 was used on customer side. Now they have a Conduction issue when they passing EMI test.
When they try RC on SW pin, it doesn't improve after try may RC value. But when they try to connect a resistance between…
Part Number: LM46001 Other Parts Discussed in Thread: LM46000 , We have an a few percent of boards failing in the field in the same way as described in the related thread. It appears that the ability for VIN to provide the initial voltage to the LDO in broken…
Part Number: LM46001 I would like to operate VOUT at 1.8V instead of 3.3V during system inactivity.
The BIAS uses the output for improved efficiency, but requires 3.3V minimum.
Will the LDO automatically switch to VIN when VOUT < 3.3V?
Or do I need…
Part Number: LM46001 Hello,
Could you please submit IMDS report for below components to Kimball Jasper IMDS account 15918. Those are urgently needed for IMDS for ZF and Knorr Bremse application.
Kimball Part#
Supplier name
IMDS Status
MPN
…
Hi Andy-san,
I appreciate your great support. This make it clear that Iq is not dependent on the switching frequency. Also, the input current is consistent with customer's evaluation result.
Regards,
Saito
Part Number: LM46001 Data sheet Section 6.8 appears to claim light load efficiency is higher at 500KHz than at 200KHz.
For 5V, 1mA load and 42Vin, the efficiencies are 67% for 500KHz and 41% for 200KHz.
Is there something else going on?