Part Number: LM46002 Other Parts Discussed in Thread: LM76002 , LM43602 Hi Sir,
Our customer product is Radio, They are need Buck solution as below.
Does TI LM46002 can be meet this SPEC? or have better solution can be shore to me?
VIN Range…
Part Number: LM46002 Tool/software: WEBENCH® Design Tools I request LM46002 as free sample from ti store footprint is dull-red,is it normal ? is it has silver color footprint?
Part Number: LM46002 Hi,
the Output voltage of the LM4002 is set to +5V. But sometimes in the first 100ms after powering up the output voltage rises up to 11V. Then it slowly comes back to 5V and then it works fine.
The capacitor Cff which is parallel…
Part Number: LM46002 Tool/software: WEBENCH® Design Tools I request free sample from ti store,found LM46002 footprint is dull-red,is it normal colour ? is it have silver footprint?
Hello,
There is a specific P-SPICE model for the LM46002 IBB topology. You can find this in the models table.
Please let me know if you have any additional questions or if anything is unclear.
Best Regards,
Katelyn
Part Number: LM46002 Other Parts Discussed in Thread: LM46001 Hi Support
There are three threads which describe the same issue with the LM46001 / LM46002LM46002: power supply stops working after 2 month x 2
LM46001: Failure in ability to power…
Part Number: LM46002 Design:
24V In
-17V Out
0.5A max
At what load should I expect the part to drop into PFM operation? How is this affected by the switching frequency set by RT?
What amount of output capacitance should I have for -17V Out…
Part Number: LM46002 Dear team,
When customers were testing, 2 of their PCBs couldn't start up. The Vcc pin was 2.7V which just meet the UVLO of Vcc. If the LM46002 was blown by a heat air gun, the IC could start up. The schematic is as followed.
…