Part Number: LM46002-Q1 Other Parts Discussed in Thread: LM46002 Hi TI expert,
May I have your help to check whether LM46002 A QPWPRQ1 has any minimum soft-start time limitation?
We would like to control the SS time within 0.5ms, so it will be lower than…
Part Number: LM46002-Q1 Hi Team,
My customer wants to know if LM46002-q1 might get damage or not, in following input voltage variation stress test. Is there a possibility that the LM46002-q1 will get a damage by the test? if you have any concerns, please…
Part Number: LM46002-Q1 Hello All,
I am designing PCB, having DCDC converter with LM46002-Q1 part.
I found one previuos board having copper removed from other side of inductor.
check attached image, showing bottom side of PCB, copper removed from area…
Part Number: LM46002-Q1 Other Parts Discussed in Thread: LM46002 Dears
When i only provide 24V input and didn't enable ti ,i found Vout has 1.7V voltage. Dose it normal output?
This moment every pin output voltage as below
my schematic as below ,pls…
Part Number: LM46002-Q1 Other Parts Discussed in Thread: LM46002 Ladies and/or Gentlemen,
We have a circuit on the drawing board powered by an LM46002-Q1 (automotive application). Worst-case load during normal operation is 368 mA @ 5 V.
Now my test department…
Part Number: LM46002-Q1
Hi Team, The datasheet shows the following however I coudn't find detail defference between LM46002-Q1 and LM46002A-Q1. >The LM46002A-Q1 version is optimized for PFM operation and recommended for new designs. Could you tell…
Part Number: LM46002-Q1 Our customer consider to use LM46002-Q1 for following inverting circuit.
VIN:5V or 10V
Vout:-17V
Iout:200mA
Fsync:460kHz-480kHz
But they don't like PFM mode of this device.
So they consider to add dummy resister to Load to…
Part Number: LM46002-Q1
CIrcuit is based off a web bench design. I added the voltage divider for the enable pin. I can see the ~3.2 volts on the VCC pin but 0V on the output. The enable pin gets above 1.2V. Red layout is the top, blue is the bottom…