Part Number: LM5005 Other Parts Discussed in Thread: LMR38020
hi team,
my customer find that when the add a pull up resistor of 75kΩ in RAMP to VCC, the Vout can't stay at 24V when they increase the output current. Do u have any advice on the case? thanks…
Part Number: LM5005 Other Parts Discussed in Thread: LM25005 , Hello,
We have a circuit board in production that uses the LM5005MH/NOPB as a 24VDC to 5.5VDC converter (0.5A to 2A depending upon application) .
Our production is halted due to the limited…
Part Number: LM5005 Dear team
The spec is Vin=56V、Vo=12V
The customer using the LM5005. But they found the output voltage(12V) is not clean, The ripple is about 952mVpp.
They add the output capacitor. but the effect is not obvious.
Could you help to review…
Part Number: LM5005
Hi,
We are using LM5005 to stepdown 36V to 14V.We are using 220uH MSS1278-224KL inductor.
This inductor is radiating noise to one of our transducer. Can you please suggest solution to suppress these radiation.
Part Number: LM5005 Dear team
Dose TI have those data of LM5005MHX ?
1.Charge device model (CDM)
2. Machine model (MM).
3. ESD Human Body Model
Many thanks
Denny
Part Number: LM5005EVAL Other Parts Discussed in Thread: LM5005 , LMR38020 Hi,
Need gerber and design files for AN-1748 LM5005 Evaluation Board. Can you please provide it.
Part Number: LM5005 Other Parts Discussed in Thread: LM5088 Hey Team,
I have a customer that has designed a board with the LM5005 and is running it at it's max, 75V. The LM5005s tend to explode after 3-4 times of power up and we can't seem to find the…
Jafar,
Your output ripple is good, the converter looks stable and it is probably not the output capacitance causing the issue.
It appears your vias under the ICs exposed pad are not connected to the GND planes.
These vias are necessary to move heat from…