Part Number: LM5010 Other Parts Discussed in Thread: TPSM365R6 Hey team,
can you please help:
We continue to use the LM5010MH/NOPB HTSSOP14 regulator in a redesign.
If this is short-circuited at the output p24V to GND and the short-circuit is removed…
Part Number: LM5010 Hi,
The test inductance in the LM5010SD/NOPB power supply circuit has been "howling", resulting in our audio acquisition equipment can recover the problem of inductance "howling".
The usage requirement is Vin 12…
Part Number: LM5010 Dear Team,
I'm currently designing a new DC-DC converter to be used in a BLDC Drive.
Since I'm new to designing, I'm doubtful to proceed with this Schematic. I've got different values in WEBENCH and LM5010 calculator Please verify…
Part Number: LM5010 I have an application where I need to diode-OR a power supply from two different sources. Is it ok to apply power to the output of a LM5010 regulator when its input is unpowered or do I need to insert a series diode in the output? …
Part Number: LM5010 Hi Andy, thanks for the reply.
Continuation of previous inquiry
I changed power suuply, I was able to output 15V.
I used 500 ohm as a dummy load, Is there a way or formula to validate the 500 ohm?
Thanks very much -yuuki
Part Number: LM5010 Hi, I'm trying to use the LM5010MH/NOPB to convert input voltages in the 24V to 48V range down to 15V. Currently, it can only output up to about 3.5V.
Here is the schematic for my circuit. I've also attached the Webench design that…
Part Number: LM5010 Use LM5010SD power supply scheme, compatible with 12VDC and 24VAV, and provide 5V output. Now that the 12V input power is working normally, the inductance "howling" in the 24VAV input power solution, what could be the problem? thank…
Part Number: LM5010Lm5010 works as 15V converter for MOSFET drivers, Vin 48V. LM5010 is followed by the Efuse TPS6623 working as protector, just in case LM dies and 48V input voltage propagates to rest of the system. The 15V is used to make 5 and 3V3…