Part Number: LM5012 Other Parts Discussed in Thread: LM5013
Hi,
Can we reduce the internal soft-start time from 3ms to 1.75ms (which is minimum as per data sheet)? If so may I know how to do that?
Regards
Ravi
Part Number: LM5012-Q1 Other Parts Discussed in Thread: LM5012 , LMR38020 Tool/software: I am using Below circuit for My BMS application.
MCU TMS320F28P659 100 PIN MCU.
LM5012 for converting 48V to 12 V
TPS62901QRYTRQ1 for converting 12V to…
Part Number: LM5012 Other Parts Discussed in Thread: LM5164 Tool/software: Dear Sir We replaced your LM5164 with a LM5012 (purchased from Mouser). Our input voltage is 75V DC. The LM5164 works flawlessly, however the LM5012 fails (when we enable it ,…
Part Number: LM5012-Q1 Other Parts Discussed in Thread: LM5012 , LM5102 , LM5013 Tool/software: Hello team,
Customer wants to know how to design the external components parameters, work conditions: 48V battery, Vout = 12V, Iout = 1.5A.
1. Non-sync…
Part Number: LM5012 Other Parts Discussed in Thread: LM5013 Tool/software: Hey, I am looking for a drop-in replacement for the LM5012 Buck convertor with a higher current draw capacity, would LM5013 work for the same. Ill change the output catch diodes…
Part Number: LM5012 Tool/software: As the title states, what happens to the LM5012 if the input voltage drops below the set output voltage? Does it pass through the voltage? Say for example the voltage output is set to 12V, and then the input drops to…
Part Number: LM5012-Q1 Tool/software:
Hi to TI support team,
i did this design, which works well now but with some emc problems.
The emc test engineer recommends, to populate a 2.2nF capacitor parallel to R21 (RT/SYNC) resistor.
He said, this…
Part Number: LM5012-Q1 Tool/software: Hello
our customer is asking for the input current of the EN/UVLO pin not mentioned in the datasheet.
My understanding: its leakage of the comparator only.
please provide some data.
best regards
Mar…