Other Parts Discussed in Thread: LM5019 Hello,
I need a high voltage buck regulator (~60V input voltage) output voltage is adjustable from ~16V to close to the input voltage. Output current is rather low ~ 100mA. I was experimenting with the LM5019…
Part Number: LMR36500 Other Parts Discussed in Thread: LM5019 Hello TI members,
Question1:
How much current (sink/source) is required on pin 3 (EN/UVLO) of LMR36500 to enable the device? I plan to use an optocoupler for controlling the EN/UVLO pin…
Part Number: TPS23882B Other Parts Discussed in Thread: LM5017 , LM5019 Hi Sir,
as far as i know , that TPS23882B1 has autonomous mode and does not need SRAM can to be compliant to the standard_802.3at and .bt , right?
customer want to do dumb switch…
Part Number: LM5018 Other Parts Discussed in Thread: LM5019 , LM34926 , LM5168 Hi Team,
Good day! I need your help and confirmation with the replacement for LM5018.
I am checking these devices below. I checked the pin out and they are the same with…
Part Number: LM34925 Other Parts Discussed in Thread: LM5018 , , LM5019 , LM34926 Hi All,
What is the difference between LM34925 and LM5018? As far as I checked the data sheet, I think it is the same. Customer is currently using the LM34925. What are…
Part Number: TPS2388 Other Parts Discussed in Thread: CSD19538Q3A , LM5019 , MSP430F5234 Hello Expert,
Our customer is considering PSE design w/ TPS2388 or TPS2388x.
So I have some questions that I have to do consider for it.
Could you please let…
Part Number: LM5017 Other Parts Discussed in Thread: LM5019 , LM5018 , LM5181 , LM5180 Hi Team,
we would like to use LM5017 to design a isolated power with flybuck topology. But in the slpc017b calculator, we find the LM5017 is not recommended in flybuck…
Hey again Lauren ,
The isolation transformer on the LM5019 EVM is the same series, Coilcraft LPD5030V-154ME so it also has a 1.5kV isolation rating. You can also use a higher isolation transformer from the magnetics vendor.
Are you specifically looking…
Dear Penny:
Thanks!
About your item 1=>Change LM5574 to LM5019.
We already design LM5574 in many other product.(54V to 3.3V).
Could you let me know your consider?
Thanks!
Caspar
Kǎolǜ
2/5000
…