Hi Yaita-san,
The LM5021-Q1 and the LM25037-Q1 are the two controllers that are most suitable for this power range and have automotive qualification.
Regards
Peter
Viktorija,
Thanks for the interest here.
This is an interesting question. I don't think we've tested this before but I don't see why it wouldn't work.
Can you help me understand why this approach is of interest?
Since it's not isolated I'm…
Dear Sir,
I'm not the writer of this application note. But here I'll give my reply from my point of view: This kind of connection is not a good connection for both opto-coupler and TL431 1) Its hard to say the 130uA source can't drive the BJT in TCMT1107…
PN Note: (-Q1) when auto PN is substituted
Description
Link
Input Voltage
Output Voltage
Output Power
OBC
EV Charging Station
DC-DC
Topology
LM5021 (-Q1) + UCC28180
PMP10215 Universal…
Part Number: LM5021 Other Parts Discussed in Thread: PMP10215 , , PMP40281 , UCC256402 Hi, TI expert,
Currently need to make a two-tube forward design with 300~1000V input Voltage, 24V output Voltage and 200W output Power.
Suppose LM5021 is the…
Part Number: LM5021
Hi,
I am using LM5021 to build wide-input dc voltage range for auxiliary power supply(24V,50W) by flyback converter.
Operation condition was 150V input and checking the each of LM5021 pins.
VIN and VCC are good and well regulated…
Part Number: LM5021 Other Parts Discussed in Thread: TINA-TI , TL431 Hi, team.
i have been asked by customer as below, please tell us
Q1.Can customer utilize TINA TI to simulate how much phase margin would be there in specific schematic ?
Part Number: LM5021 Hi, Team.
Q1.
is there any maximum value Customer can use the cap value on SS pin?
Q2.
for disabling skip cycle, what customer has to do is only "having 125mV" on CS pin? any other thing customer has to care ?