Part Number: LM5036 Hi Team,
I am trying to design a power supply based on LM5036, but i found that there is no isolation cap on EVM, how does the LM5036 prevent the transformer saturation?
BRs,
Thank you
Part Number: LM5036 Hi team we are considering making a project using lm5036. But we have a question about one thing.
How can we perform the on/off operation safely via an external mosfet?
also UNVLO, OVP, OTP and CBC protections must also be functioning…
Part Number: LM5036 Hi,
It looks like we are seeing a serious reliability issue on the internal auxiliary power inside LM5036.
The outputs of the auxiliary power (VCCP,VCCS) are not correct after long time power on/off test under -40C. (auxilary power…
Part Number: LM5036 Other Parts Discussed in Thread: UCC28251 Hello,
I´m looking for a controller for a half-bridge isolated buck converter. The input voltage is much higher than the allowed 100V written in datasheet. Is it possible to use a external…
Part Number: LM5036 Hello
Our application is DC/DC converter, topology is half bridge and the input is 48V, we observed abnormal behavior during on/off test with LM5036, see below.
at normal conditions, the SR1 is complement to LSG.
but sometimes we observe…
Part Number: LM5036 Hi team
Customer is using LM5036 in 500W power module, 18~36VDC in, but we found an issue when shut down with no load.
Yellow is VOUT, Pink is SR, Green is SSSR.
We suppose that it's due to zero duty operation, when in no load, you…
Part Number: LM5036 Other Parts Discussed in Thread: LM5035C Hi Team,
Can you please help us with our customer's inquiry below?
I will not use a secondary rectifier and an aux power supply. Is it necessary to install the components that determine…
Part Number: LM5036 Other Parts Discussed in Thread: UCC28951 , UCC25800 Hi team,
My customer has a question regarding LM5036.
As the dead-time is calculated as, t1 = tD + tCLK
while tD = RD1 × 2 pF + 20 ns
And tCLK is typically 65ns.
The total deadtime…