Part Number: LM5046 Other Parts Discussed in Thread: UCC28950 Tool/software: Hi,
I read the LM5046 datasheet and while using the provided XLSX calculator I noticed something strange:
When calculating R1 R2 R3 i get very different results when compared…
Part Number: LM5046 Other Parts Discussed in Thread: UCC28950 , LM5026 , UCC28630 , UCC28782 Tool/software: Hello, Team,
Customer contacted us about using LM5046 in their new R&D project of H-Bridge DCDC Converter. They plan to use it in current mode…
Part Number: LM5046 Hey All,
I have a question about the LM5046 (Phase-Shift Controller), I am doing current control for the PSFB application, I checked that the COMP pin takes input as current, Is there any other way to converter voltage equivalent…
Part Number: LM5046 Tool/software: Hi,
So i was looking at the LM5046 chip and i was studying this document and i could not find the transformer core used in this design.
What ER? cor was used was it ungapped or not?
Also do you think FB can be…
Part Number: LM5046 Other Parts Discussed in Thread: LM5035 Tool/software: Hello E2E Experts,
Good day.
In LM5046 and LM5035, there is no Dmax. I can't calculate the switching frequency. So these components can make up to 2MHz oscillator frequency…
Part Number: LM5046 Hi All,
I have a question regarding the output of the LM5046, the datasheet says the duty can vary from 0-100% with the COMP pin varying between 1 mA to 0 mA. In my design, the switched voltage waveforms of the PSFB converter reach…
Part Number: LM5046
Hi everyone,
I am currently working with the IC LM5046MH/NOPB and trying to achieve a phase shifted full bridge operation. I am trying to generate the phase shifted PWM pulses for the switching MOSFETs. I am able to achieve the…
Part Number: LM5046 Other Parts Discussed in Thread: LM5045 , We currently use LM5045 in full bridge DC-DC converter; the Xfmr sec. output is a single winding and it too is a full bridge topology using 4 synch rectifiers controlled by two UCC21225's,…
Part Number: LM5046 Hi All,
I'm using LM5046 for a custom application which involves running the oscillator at ~2MHz (RT Resistor = 4.7K), hence the PWMs at 1 MHz. With this, I have connected the output of LM5046 (LO1/HO1, LO2/HO2) to the gate driver…