Part Number: LM5113 Hi,
in designing a Class-D audio amplifier I encounter a topic which I do not understand.
The circuit depicted below has been simplified for debugging reasons. The input signals for the LM5113 (PWM_LEFT_Delay and PWM_INV_LEFT_Delay…
Part Number: LM5113 Other Parts Discussed in Thread: LMG1205 Hi,
in the data sheet of the LM5113 external R and C are shown in Fig. 16 (" Feature Description"). I am not shure, whether the R and C have to be adapted externally or whether they are included…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113 , UCC27624 , LMG1205 , LMG1025-Q1 Hi, I'm Takamoto Furuichi, DENSO Corp.
I have the question about the LM5113's spec.
We have confirmed that the following turnon delays tend to depend…
Hello Aidan,
Any request looking into the LM5113 internally results in the definite recommendation to add the external boot diode and 20 ohm resistance. I think there are improvements in the newer GaN drivers to address the boot diode operation which…
Part Number: LM5113-Q1
Hi, I'm Takamoto Furuichi, DENSO Corp.
We would like to ask about the fluctuation of the charactoristics due to the external stress.
If you have the data of "turn on propagation deley" vs "external stress" or "…
Part Number: LM5113 Other Parts Discussed in Thread: LMG1205 , Hi together,
we usethree LM5113 in our 3-phase inverter design with EPC2022 GAN-Fets. We do not use any gate-resistors neither for turn-on nor turn-off. Furthermore we don´t have any filter…
Part Number: LM5113 Hi,
Looking at the UVLO rising thresholds on the LM5113 I noticed a discrepancy on the VHB-VHS when comparing the typical electrical characteristics and the characteristics over temperature.
On the typical characteristics it specifies…
Hey Nikita,
I am still investigating this and will get back with you on the findings but I just want to confirm, are you using the LM5113 or the LM5113-Q1?
Currently, the LM5113 is not recommended for new designs as indicated on ti.com, but the LM5113…
Part Number: LM5113 Hello, if we are only using the low side driver in the LM5113, should we leave the HB, HOH, HOL, HS pins not connected, or grounded?
Part Number: LM5113 I saw that d/s recommends to use external bootstrap diode and 20 Ohm resistor. But there is application circuit does not have this bootstrap circuitry.
Is this necessary? and what's the benefit of this external bootstrap?