Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113 , UCC27624 , LMG1205 , LMG1025-Q1 Hi, I'm Takamoto Furuichi, DENSO Corp.
I have the question about the LM5113's spec.
We have confirmed that the following turnon delays tend to depend…
Part Number: LM5113-Q1
Hi, I'm Takamoto Furuichi, DENSO Corp.
We would like to ask about the fluctuation of the charactoristics due to the external stress.
If you have the data of "turn on propagation deley" vs "external stress" or "…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LMG1025-Q1 ■ Target: LM5113-Q1, LMG1025-Q1 ■ Desired data: Temperature characteristics of propagation delay time ⇒Propagation delay time at -40, 25, 150℃ and its variation. In addition, I would…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113
My question is on the
Lm5113 part , the Tmon and Tmoff shows a delay matching of 1.5ns typical max 8ns I have a few questions
What is the output impedance of the driver during that “dead…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113 Dear,
We chose LM5113 as the gate driver for GS1008P in our class-d audio amplifier (CDA), and there's a phenomenon we can't explain. We think the gate driver may cause it. Our CDA…
Part Number: LM5113-Q1 hi Datasheet says HS pin has -5V Abs max rating, is this DC ratings?
when the HS is pulled lower than -5V, what is possible damage? would it be ESD cell damage or different damage mode?
Hey Nikita,
I am still investigating this and will get back with you on the findings but I just want to confirm, are you using the LM5113 or the LM5113-Q1?
Currently, the LM5113 is not recommended for new designs as indicated on ti.com, but the LM5113…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113 To team
Please share the drawing of thermal PAD for LM5113-Q1. This data is not on the Datasheet.
Best regards,
Daisuke Nomura
Hey William,
thank you so much for your fast response.
the Class-D amplifier uses a 3-level (or 3-point) PWM. Unlike in a 2-level PWM, both high side switches (MOSFETs) or both low side switches may be activated simultaneously. This happens when the input…
Hey Clemens,
Thank you for the waveforms and the updates.
As a reminder, the LM5113 is no longer recommended for new designs as noted on the product page. The LM5113-Q1 is still an active part in the WSON-10 package and the LMG1205 is an active part in…