Part Number: LM5117 Hello, My LM5117 converter is designed to step-down a 18V (5-cells) Li-ion battery voltage to 15.8V for a powertool that usually accepts a 14V (4-cells) Li-ion battery. Max current is 80A during 100ms.
When I test my design with…
Part Number: LM5117-Q1 Other Parts Discussed in Thread: LM5117 Tool/software: Hello I am using LM5117 with switching freq 480KHZin my ECU during Radiated emission in 966KHZ and 160MHZ. When I checked with near field probe I am getting the emissions source…
Part Number: LM5117-Q1 Tool/software:
LM5117QPMHX_NOPB gate resistance can be tuned to 9 ohm without compromising working and efficiency of buck
When there is no load connected to LM5117QPMHX_NOPB buck, why there is more emission at 960kHz. What is…
Part Number: LM5117-Q1
Tool/software:
I am using LM5117PMHX/NOPB IC and following this schematic from LM25117 Evaluation Board .
I designed it for 12V output but I am getting ~2.7V output which is a problem, I have tried few solution but nothing…
Part Number: LM5117-Q1 Other Parts Discussed in Thread: LM5190 Tool/software: Hello Team,
We are using LM5117-Q1 in one of product. We want to check whether LM5117-Q1 is suitable for Super Capacitor charging application with below specifications:…
Part Number: LM5117 Other Parts Discussed in Thread: TINA-TI , CSD19536KTT Tool/software: Hi all,
I'm simulating an High Current DC-DC based on LM5117 but I got a lot error message for convergence failed.
I start with the Excel File (attached) for…
Part Number: LM5117 Tool/software: [Repeating info already posted on a locked thread]
On a few instances, we have experienced a failure of the LM5117 Buck Controller, which surprised us since we expected the failure in this circuit to be the thermal…
Part Number: LM5117 Tool/software: On a few instances, we have experienced a failure of the LM5117 Buck Controller, which surprised us since we expected the failure in this circuit to be the thermal-heavy components (NFET, Inductor, sense resistor, etc…
Part Number: LM5117 Tool/software: In my CC/CV DC-DC converter project I need to put 2 MOSFET in parallel to manage more current and I need a very high peak current to charge quickly the two gates, so I choose le LM5117 because it has 2.2Amps Gate peak…