Part Number: LM5118-Q1 Other Parts Discussed in Thread: LM5118 , LM51770 Tool/software: Hi Community,
I use the LM5118-Q1 for my power supply and I have two issues :
I have whistling when I need 58V 2A in output (24V on input). To remove it, I have…
Part Number: LM5118 Tool/software: Hi Team,
Can you suggest a method to calculate the power dissipation of the LM5118MH during both operation and no-load conditions?
Thanks & Regards
Thirupathi T
Part Number: LM5118 Other Parts Discussed in Thread: INA237 Tool/software: Hi Team,
Kindly review the attached schematics and PCB Layout for a custom board and provide your feedback on the same.
PCB_Images.zip
PoE_Boost_Schematics.pdf
The attached…
Part Number: LM5118 Tool/software: Hi, I am working on a prototype for a wide input voltage to 5v @ 1A power supply. I am finding that my prototype fails to regulate when VIn passes below VOut. Specifications: In: +4v to +48v Out: +5v @ 1A Freq: 407 kHz…
Part Number: LM5118 Tool/software: I have a board using the LM5118MHX/NOPB in a buck-boost mode. The part seems to have failed: 1. There is power at Vin. 2. The enable pin is high (14V) 3. There is no output from Vcc pin (0V). I am looking for verification…
Part Number: LM5118 Tool/software: Hi TI community,
I’m working on an LM5118 design with the following specifications and I’m having a hard time finding a suitable inductor. I’m not that experienced in power electronics and hope someone would like to…
Part Number: LM5118-Q1 Tool/software: Hi Stefan, Hope you are doing well. I am sharing, all the waveforms issues i am facing is on comp and ss on low input 15V the output trips / clamp to 18V which was wrong as i had design it for 23V out however on higher…
Part Number: LM5118 Tool/software: Hi E2E, It is possible to acquire a non-password protected version of the Quick Start Component Calculator for the LM5118(snvu065a)? I'm curious how the excel sheet calculate some of the equation, as the datasheet is…
Part Number: LM5118 Tool/software: Hi Sir, could you help us double confirm this schematic is ok? about LM5118, initially it seems ok.
ZGHN-0401DOR_POE-V01_schematics - 編輯PDF.pdf