Hi Stefan,
One of my coworkers has been working on a different solution and he is getting good results, so we are going to move forward with his design. Thanks for all of your help with debugging my problems.
Garrett
Part Number: LM5118EVAL Other Parts Discussed in Thread: LM5118 Hi,
i have been working on this board (LM5118 Wide Voltage Range Buck-Boost Controller). I have a question please!
and my question is: can it be posible to implement a reverse polarity on…
Part Number: LM5118EVAL Other Parts Discussed in Thread: LM5118 Hi TI team,
How are you doing? To speed up the design integration, could you help to provide the Design files for LM5118EVAL? At its page, only PDF files are available. Thank you.
Part Number: LM5118EVAL Other Parts Discussed in Thread: LM5118 Greetings!
We have procured LM5118EVAL/NOPB. It is designed to provide an output of 12V with 3A. We require an output of 7.4V . Since LM5118 is capable of this, is it possible to achieve this…
Part Number: LM5118EVAL Other Parts Discussed in Thread: LM5118 Team,
Please help address my customer's questions:
I want to modify the parameters on the LM5118EVAL board. I am not sure the TI experts will have any concerns:
At EN pin, I will put…
Part Number: LM5118EVAL Other Parts Discussed in Thread: LM5118 Hello All,
I bought the LM5118 evaluation board and now I am trying to get a (12 V at 1 A) output.
I connected a resistor load at the output and apply the voltage from 5 to 15V to the input…
Part Number: LM5118EVAL Other Parts Discussed in Thread: LM5118 , Tool/software: Webench Hello,
for an application with Vin from 8 to 75 VDC I have developed an identical circuit board to the all'evalution board LM5118EVAL. The maximum current in each case…
Other Parts Discussed in Thread: LM5118 Hi there,
i'm seriously interessted in the Evaluation Board AN-1819 LM5118. I got some questions about this module. What i need is a buck/boost-converter which provides a output of 10 A. Is it possible to modificate…
Hi Sir,
The customer would to design this DC-power device on the industrial and automotive products, the MP schedule is Y2023.
If the 10A is really high for diodes on 2-switch design, may I recommend the customer to use the 4-switch design same as the…